Wiki pages that were migrated are redirecting to the new location. Pages not migrated are only accessible to users on the TI network. Users off the network can not access the Wiki and will receive a 404 error. DO NOT share Wiki URLs with customers. They can not access the Wiki site.
Connecting To An LCEVM with CCS
Contents
[hide]Overview[edit]
This page discusses the procedure for connecting to one of the 64x+ or 66x Low Cost EVMs with an emulator via Code Composer Studio. The Low Cost EVMs come with an on-board XDS100, and some will also have a Mezzanine XDS560v2 Emulator attached to them. If your board has a Mezzanine Card attached to it, take note of the XDS560v2 Mezzanine Emulator Considerations below.
This article focuses only on the two on-board emulation options for LCEVMs. You can also connect with a 3rd party emulator via the 14-pin or 60-pin emulation connector. Contact the emulator supplier for assistance with connecting in this manner.
| If your EVM has a 60-pin emulation header on-board, there is no 14-pin header that will allow connection to the DSP. Some of the boards will have a 14-pin header implemented along with a 60-pin header. In these cases, the 14-pin header is not connected to the DSP scan chain. |
Emulator Considerations[edit]
| On-Board XDS100 Considerations |
|---|
The following considerations should be noted if you are using the On-Board XDS100 emulation
|
| Mezzanine Emulator Considerations |
|---|
The following considerations should be noted if your LCEVM came with an XDS560v2 Mezzanine card mounted to it.
|
Setting Up CCS for the on-board XDS100[edit]
|
| Adding a GEL file to be automatically loaded |
|
| CCSv5 Target Configuration (XDS100) |
The following instructions are shown for configuring CCS to connect to the C6678 LCEVM. The only difference for any of the other LCEVMs is the choice of the device.
- Create a New Target Configuration in CCS
- File -> New -> Target Configuration File
- Select Texas Instruments XDS100v1 USB Emulator
- Choose the Appropriate Target Device
- Optional - Attach GEL files to one or more cores
- Click the Advanced Tab
- Select a CPU to add a GEL file to
- Use the browse button next to the Initialization Script dialog to point to the appropriate GEL file.
- Repeat as necessary for each core.
- Save the Configuration
Setting Up CCS for the Mezzanine Emulator[edit]
|
| CCSv5 Target Configuration (XDS560v2 Mezzanine) |
The following instructions are shown for configuring CCS to connect to the C6678LE EVM with on-board XDS560v2 Mezzanine Emulator. The only difference for any of the other LCEVMs with on-board XDS560v2 is the choice of the device.
- Create a New Target Configuration in CCS
- File -> New -> Target Configuration File
- Select Texas Instruments XDS100v1 USB Emulator
- Choose the Appropriate Target Device
- Optional - Attach GEL files to one or more cores
- Click the Advanced Tab
- Select a CPU to add a GEL file to
- Use the browse button next to the Initialization Script dialog to point to the appropriate GEL file.
- Repeat as necessary for each core.
- Save the Configuration
The Most Common Mistakes[edit]
- If you are trying to use the on-board XDS100, be sure that there is nothing connected to the 60-pin emulation header on the board. Common issues are:
- A 14-60 pin adapter left connected to the header
- Mezzanine Card connected to the Emulator. (If your EVM has a mezzaznine emulator built on it, you MUST use the Mezzanine Emulator. XDS100 emulation is disabled.
- Make sure that you have selected the correct emulator in the target configuration.
- If you are using a Mezzanine, make sure that the selected emulator is "Blackhawk XDS560v2 Mezzanine".
- If you are using the on-board XDS100, make sure you have selected "XDS100v1".